Back to Maintenance Manager for Manufacturing Main Menu

Printing a Work Order

Administrators and Technicians can print the work order details or save them as a PDF or other supported format in Maintenance Manager for Manufacturing (MMM).

To print a work order

  1. Navigate to the (Work orders) page.

  2. Click a work order.
    The work order panel opens.

  3. Click the icon at upper right corner of the work order panel.

  4. Click Print Work Order.

  5. From the Destination drop-down list, select the desired output format.

  6. Additionally, configure the following print settings, as required:

    • Pages

    • Page per sheet

    • Margins

    • Options

  1. Click Save to print a work order in PDF.

  2. Browse to the desired location, and then select Save.

  3. The work order is saved as a PDF file in the selected location.